CAP#.PREEDGE
Description
If precondition mode 1 has been selected, then this selects which edge of the precondition input will be waited for before the trigger is allowed.
Examples
Usage
1: Rising edge (default)
2: Falling edge
3: Rising or falling edge
Code
-->CAP1.EDGE 1 -->
Context
See Capture.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 3 |
|
Default Value |
1 |
|
Data Type |
Integer |
| See Also | CAP#.PREMODE, CAP#.PRESELECT |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
CAP1.PREEDGE |
4400h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
CAP2.PREEDGE |
4401h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
31040 |
1 |
31040 (0x7940) |
CAP1.PREEDGE |
Unsigned8 |
Read/Write |
Yes |
|
31041 |
1 |
31041 (0x7941) |
CAP2.PREEDGE |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
CAP1.PREEDGE |
31040 |
Unsigned8 |
Read/Write |
- |
|
CAP2.PREEDGE |
31041 |
Unsigned8 |
Read/Write |
- |
Related Topics